DA16200 not probed in linux

Hi Team,

My platform is TI AM62x processor . Linux kernel is 6.1.33, driver version is  v5.2.1.2, use the sdio interface 

After I insert the driver, the initialization function returns 0, indicating that there is no error in initialization.

But the probe function did not run . What could be the reason?

Parents Reply
  • Hi ST,

    Apologies for the delay.
    Please find the answers from the Wi-Fi Support Team:
    1. No. You do not need to rewrite an image. TO run the DA16200 with the Linux driver, the entire contents of the flash memory should be erased first. The linux driver will download the firmware to the DA16200.

    2. Without the details of the custom Yocto, we cannot provide exact configurations that need to be ported to a custom Yocto.

    3. It seems that the driver cannot get the MAC address from DA16200. We think that the status of the CD pin should be checked to see if it is low or not. To proper operation, the CD pin should be low. Please refer to the user manual on section 4.7.1
    UM-WI-059 DA16200 DA16600 Linux Driver Getting Started Guide (renesas.com)

    If you have any further questions, please let us know. Please also check your Private Messages and share with us some details there as well.

    Best Regards,
    OV_Renesas

Children
No Data