DA16600 firmware download

Hello,

I am using DA16600 for my project. I want to develop a system to update the DA16600 firmware on-field. 

I referred the documentation and implemented Y-Modem protocol. Everything works fine, except for the last packet.

According the the protocol used, packet size is 1024 bytes. there will be a case where, the last packet will be smaller and padding has to be done. In my code, padding is done with '\0' byte, but when same firmware is downloaded with multidownloader tool, padding bytes are different. please refer the attached file [time marker '0' marks the end of firmware file and the rest are padding bytes].

7534.refer.zip

folder contains 3 files;

1. CP145_WIFI_RTOS.img [firmware image used, this is RTOS image renamed manually]

2. fw_update_manual.sal [this is a capture of programming the DA16600 using my MCU]

3. fw_update_multidownloader.sal [this is a capture of programming the DA16600 using multidownloader tool]

how to generate these padding bytes ? can you direct me to a documentation mentioning this ?

Thank you.

Kind regards,

synd223

Parents
  • Hi Synd,

    Could you check on the freertos-sdk-programmer-guide section 15:

    UM-WI-046 DA16200 DA16600 FreeRTOS SDK Programmer Guide

    BR,

    JH_Renesas

  • Hi JH_Renesas,

    I read the documentation 'UM-WI-046', but I do not see a reference to the question I raised, it contains information about OTA firmware updates. I can confirm that the OTA updates are working fine, but my primary concern is with programming the DA16600 using debug lines using the Y-Modem protocol. 

    I am following the procedure used by the multidownloader tool, everything is correct except the ending part. The last packet contains some unknown characters [padding bytes] when programmed using multidownloader tool,

    I want to know if there is some syntax being followed or just some random bytes!! Is there any method to generate these bytes ? can I use null characters instead ? 

    The main reason for raising this issue is because these bytes are same everytime I program using the tool, and with a different firmware the padding bytes are different. 

    Please give me more information regarding this concern.

    Thank you. 

    Regards,

    synd223

Reply
  • Hi JH_Renesas,

    I read the documentation 'UM-WI-046', but I do not see a reference to the question I raised, it contains information about OTA firmware updates. I can confirm that the OTA updates are working fine, but my primary concern is with programming the DA16600 using debug lines using the Y-Modem protocol. 

    I am following the procedure used by the multidownloader tool, everything is correct except the ending part. The last packet contains some unknown characters [padding bytes] when programmed using multidownloader tool,

    I want to know if there is some syntax being followed or just some random bytes!! Is there any method to generate these bytes ? can I use null characters instead ? 

    The main reason for raising this issue is because these bytes are same everytime I program using the tool, and with a different firmware the padding bytes are different. 

    Please give me more information regarding this concern.

    Thank you. 

    Regards,

    synd223

Children