Connect wifi in da16200 and http post restart

Hello, I i refer documents UM-WI-046 DA16200 DA16600 FreeRTOS SDK Programmer Guide & getting started guide. I want to control wifi connection means i want to make my own application in that i can connect with any wifi i want if i have ssid and password of that wifi so i got that there is sample_preconfig file in which there is wifi api code in that i chnge ssid and password and try wo connect them> i have some questions:
1) in da16200 tfoldeer in e2 studio there is no file like sample_preconfig but in ADC_sample example folder that ffile is present so i capy that code and make a new file in da16200 folder and run that code also in user_main.c i call sample_preconfig() function so it is correct way  beacuse i got below output in this is this correct or not ???
  

2) Another question is now i want to do that i connect this wifi, now i want to do http post data on my server but is this way correct or not of wifi connection?because after i did same way i got issue and my renesas got stuck while go in http post function and it restart 
3)Also i got to know that i did not get ip after connecting wifi so i did dhcp renewl so after i got this output and corrected ip is this way also corrected???

  • Hi Kavan,

    Thank you for posting your question online.
    Let me check on this and I will get back to you as soon as possible.

    Best Regards,
    OV_Renesas

  • Hi Kavan,

    1) in da16200 tfoldeer in e2 studio there is no file like sample_preconfig but in ADC_sample example folder that ffile is present so i capy that code and make a new file in da16200 folder and run that code also in user_main.c i call sample_preconfig() function so it is correct way  beacuse i got below output in this is this correct or not ???

    As shown in the UART0 debug logs, you were able to establish a Wi-Fi connection so that is correct.


    2) Another question is now i want to do that i connect this wifi, now i want to do http post data on my server but is this way correct or not of wifi connection?because after i did same way i got issue and my renesas got stuck while go in http post function and it restart 

    On the UM-WI-046, please refer on section 14.5 HTTP Client. 
    You will find the example project inside the SDK and a description of the APIs being used. You will need to implement this on your project as well.
    Please share the full UART0 logs with timestamp if you are facing any crashes so we can get a better understanding.


    3)Also i got to know that i did not get ip after connecting wifi so i did dhcp renewl so after i got this output and corrected ip is this way also corrected???

    Using DHCP is the standard way to have your IP assigned. But it depends on your application scenario.

    Best Regards,
    OV_Renesas