Import TLS Server sample application in e2studio

Hi,

I tried to import a project for the Import TLS Server sample application (~/SDK/apps/common/examples/Network/TLS_Server/projects/da16200) ,  

Problems:

Parents Reply Children
  • Hi,

    thank you for your support. I solved the previous problem by selecting a short root directory when I imported the project and now I build the project successfully. I flashed the two images using the macro in Tera Term.

    the following image it says failt to initialize WLAN. What is meant by "failt to initialzie WLAN", TEST mode?

    To test the TLS connection, should I acquire the IP address with AT commands? 

  • Hi There,

    Thank you for the reply.
    1) Please refer on the UM-WI-046 DA16200 DA16600 FreeRTOS SDK Programmer Guide for a high level description of the examples on the SDK and an explanation of the APIs being used.
    2) In order for the TLS Server example to start running you will have to be connected to a network and have a TLS Client running as well.
    On my side I loaded the TLS Server example on the DA16200MOD EVK and I used the 'setup' command on the UART0 to connect to a local Network.
    I then proceeded to Import the TLS Client example and made the following changes on tls_client_sample.c file:

    #define TLS_CLIENT_SAMPLE_DEF_SERVER_IP_ADDR	"192.168.86.4"
    #define TLS_CLIENT_SAMPLE_DEF_SERVER_PORT		TLS_CLI_TEST_PORT
    
    //and on sample_defs.h file
    #define TLS_CLI_TEST_PORT					10197

    I compiled the TLS Client example and then loaded the image on the DA16600MOD EVK.
    I used again the setup command on UART0 in order to connect into the same network and there was a TLS Handshake.
    DA16200MOD TLS Server UART0 Logs:
    Wakeup source is 0x4
    [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    
    
            ******************************************************
            *             DA16200 SDK Information
            * ---------------------------------------------------
            *
            * - CPU Type        : Cortex-M4 (120MHz)
            * - OS Type         : FreeRTOS 10.4.3
            * - Serial Flash    : 4 MB
            * - SDK Version     : V3.2.8.1 GEN
            * - F/W Version     : FRTOS-GEN01-01-2aa77df370-006629
            * - F/W Build Time  : Feb  5 2025 11:15:31
            * - Boot Index      : 0
            *
            ******************************************************
    
    
    System Mode : Station Only (0)
    >>> Start DA16X Supplicant ...
    >>> DA16x Supp Ver2.7 - 2022_03
    >>> MAC address (sta0) : ec:f0:f9:ec:dd:66
    >>> sta0 interface add OK
    >>> Start STA mode...
    [atcmd_transport_set_max_session:9488]Set max session(8), max CID(9)
    [atcmd_network_get_sess_info:10549]Load sess_info(len:1240, cnt:10)
    
    >>> UART1 : Clock=80000000, BaudRate=115200, FlowControl=0
    >>> UART1 : DMA Enabled ...
    
    Start AT Command
    [atcmd_network_delete_sess_info:10603]Start
    RTC switched to XTAL
    
    !!! No proper APs found - It will be try again !!!
    
    
    >>> Network Interface (wlan0) : UP
    >>> Associated with c2:e6:9e:ab:2b:83
    
    Connection COMPLETE to c2:e6:9e:ab:2b:83
    
    -- DHCP Client WLAN0: SEL(6)
    -- DHCP Client WLAN0: REQ(1)
    -- DHCP Client WLAN0: CHK(8)
    -- DHCP Client WLAN0: BOUND(10)
             Assigned addr   : 192.168.86.4
                   netmask   : 255.255.255.0
                   gateway   : 192.168.86.170
                   DNS addr  : 192.168.86.170
    
             DHCP Server IP  : 192.168.86.170
             Lease Time      : 00h 59m 59s
             Renewal Time    : 00h 29m 59s
    
    [tls_server_sample] Start of TLS Server sample
    
    Loading the server cert. and key...ok
    Bind on tls/*:10197...ok
    Seeding the random number generator...ok
    Setting up the TLS structure...ok
    Waiting for a remote connection...>>> SNTP Server: pool.ntp.org (44.32.63.52)
    
    >>> SNTP Time sync : 2025.02.05 - 10:03:00
    ok
    Performing the TLS handshake...ok
    < Read from client:

    DA16600MOD TLS Client UART0 logs:
    Wakeup source is 0x4
    [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    
    
            ******************************************************
            *             DA16600 SDK Information
            * ---------------------------------------------------
            *
            * - CPU Type        : Cortex-M4 (120MHz)
            * - OS Type         : FreeRTOS 10.4.3
            * - Serial Flash    : 4 MB
            * - SDK Version     : V3.2.8.1 GEN
            * - F/W Version     : FRTOS-GEN01-01-2aa77df370-006629
            * - F/W Build Time  : Feb  5 2025 12:00:20
            * - Boot Index      : 0
            *
            ******************************************************
    
    
    System Mode : Station Only (0)
    >>> Start DA16X Supplicant ...
    >>> DA16x Supp Ver2.7 - 2022_03
    >>> MAC address (sta0) : d4:3d:39:12:e7:fe
    >>> sta0 interface add OK
    >>> Start STA mode...
    
    >>> UART2 : Clock=80000000, BaudRate=115200
    >>> UART2 : DMA Enabled ...
    RTC switched to XTAL
    
    !!! No proper APs found - It will be try again !!!
    
    
    >>> Network Interface (wlan0) : UP
    >>> Associated with c2:e6:9e:ab:2b:83
    
    Connection COMPLETE to c2:e6:9e:ab:2b:83
    
    -- DHCP Client WLAN0: SEL(6)
    -- DHCP Client WLAN0: REQ(1)
    -- DHCP Client WLAN0: CHK(8)
    -- DHCP Client WLAN0: BOUND(10)
             Assigned addr   : 192.168.86.65
                   netmask   : 255.255.255.0
                   gateway   : 192.168.86.170
                   DNS addr  : 192.168.86.170
    
             DHCP Server IP  : 192.168.86.170
             Lease Time      : 00h 59m 59s
             Renewal Time    : 00h 29m 59s
    
    [tls_client_sample] Start of TLS Client sample
    
    Connecting to tcp/192.168.86.4:10197...ok
    Setting up the TLS structure...ok
    Performing the TLS handshake...>>> SNTP Server: pool.ntp.org (162.159.200.123)
    ok
    < Read from server:
    >>> SNTP Time sync : 2025.02.05 - 10:03:11
    


    The AT Command feature is not enabled by default in the SDK examples.
    You will have to go on the config_generic_sdk.h file and define the __SUPPORT_ATCMD__ macro.

    If you want to test TLS Server/Client via AT commands, you just need to define the __SUPPORT_ATCMD__ macro to enable the AT commands feature and then use the other COM port to establish a connection and use the TLS related AT commands.

    Best Regards,
    OV_Renesas