DA16200 e2studio J-Link Printf()

Hello,

i use a LP WiFi click board from Mikroe with a DA16200MOD-AAC4WA32 on it and as flasher + debugger probe a Segger j-link Plus.

The connection between the j-link and the DA16200 works perfectly. I can see the RTT output on Segger RTT viewer and also in e2studio telnet terminal (localhost:19021).

With a USB to UART converter connected to UART0 of the DA16200 i see the output in e2studio serial terminal. But i cannot see the output of the Printf() code lines anywhere.

I wish only to connect my Segger j-link probe to the DA16200, so i have the following questions:

1. Is it possible to see the output of UART0 about the Segger j-link emulator in e2studio directly? Because actually i need to connect a USB to UART connector and my j-link probe to my pc.

2. How can i see the output of the Printf() code lines in e2studio?

Also the question, is it recommended to use the DA16200MOD-AAC for new designs, how long will it be available?

Thanks!

Parents Reply Children