Hi,
I'm working with the DA16200 Dialog Semiconductor kit and I have configured DA16200 as a TLS server using the example project "tls_server_sample".
".
The setup currently handles one client using mbedtls_net_accept() and mbedtls_ssl_handshake() functions.
() functions
However, I'd like to understand how to detect more than one TPC/IP client connection . Specifically:
How can I detect when a second client tries to connect to the server?
What's the best way to queue or reject additional connections once one client is active?
If it is allowed only one TLS client at a time, what's the recommended method to enforce that?