Captive portal page

Hello,

I'm currently working with the DA16200MOD and using the DA16200_DA16600_FreeRTOS_SDK_v3.2.9.2.

Is it possible to start an HTTP server while the DA16200 is in Soft AP mode?
For example, if I set the IP address of the DA16200 to 10.10.0.1 in Soft AP mode, is it possible to run an HTTP server and serve a web page when accessing 10.10.0.1 from a browser?

Any guidance or code snippets would be very helpful.

Note: I am not using AT commands. I am working directly with the DA16200 API functions provided in the SDK.

Thank you in advance!

Parents
  • Hi Df,

    Thank you for posting your question online.
    I just saw that you asked this as a follow-up on: Dynamic HTML web server - Wi-Fi - Renesas Wireless Connectivity - Renesas Engineering Community
    Apologies for the delay, I had missed this.

    Is it possible to start an HTTP server while the DA16200 is in Soft AP mode?

    From our side we had tested HTTP Server in Soft AP Mode in the past and we did not see any issues. 
    IF you want to start HTTP Server at Soft AP mode without ATCMD, you have to enter "http-server start" in the UART0 (Debug Console interface) then you can access the index.html of the server.

    Did you face any specific issues while trying to implement this?


    Best Regards,
    OV_Renesas

  • Hi OV_Renesas,

    Thank you very much for your reply.

    My idea is to have a single button, and if that button is pressed during startup, I want to set the DA16200 to Soft AP mode. If the button is not pressed, the DA16200 should perform its normal functionality (for example, measuring and displaying temperature).
    The Soft AP mode would be used only for setting Wi-Fi credentials and other configuration settings using web page (http server). So, I hope it's possible to change the Wi-Fi mode using some SDK function?

    What I need is a captive portal, as I mentioned earlier. This means that the DA16200 should be in Soft AP mode, and when I connect to its access point, a web page should automatically open in the browser (with the HTTP server running) at the IP address of the DA16200 Soft AP.

    For example, in the figure below, you can see that I have set the IP address of the DA16200 in Soft AP mode to 10.10.0.1, and the HTTP server has started.

    However, when I connect to its AP and enter 10.10.0.1 in the browser, the web page is not served.

    If nothing else, is there a way to set the IP address of the HTTP server so that it only runs on the IP address I assigned?

    I also attempted to enter the command you suggested, but I received a 'no such command' error.

    Best regards,

    df

  • Hi DF,

    Thank you for the reply.

    The Soft AP mode would be used only for setting Wi-Fi credentials and other configuration settings using web page (http server). So, I hope it's possible to change the Wi-Fi mode using some SDK function?

    Please refer on UM-WI-046 DA16200 DA16600 FreeRTOS SDK Programmer Guide




    I also attempted to enter the command you suggested, but I received a 'no such command' error.

    Based on the UART0 logs you shared the HTTP Server was already started. The command can be used on the Getting Started example where the HTTP Server is not automatically started.


    If nothing else, is there a way to set the IP address of the HTTP server so that it only runs on the IP address I assigned?

    From my understanding, it is only possible to set a specific IP address when you are working with HTTP Client.
    For the HTTP Server you could try to modify on the httpd.c file:

    httpd_init_pcb(struct altcp_pcb *pcb, u16_t port)
    {
      err_t err;
    
      if (pcb) {
        altcp_setprio(pcb, HTTPD_TCP_PRIO);
        /* set SOF_REUSEADDR here to explicitly bind httpd to multiple interfaces */
        err = altcp_bind(pcb, IP_ANY_TYPE, port);
        LWIP_UNUSED_ARG(err); /* in case of LWIP_NOASSERT */
        LWIP_ASSERT("httpd_init: tcp_bind failed", (err == ERR_OK) || (err == ERR_USE));
        pcb = altcp_listen(pcb);
        LWIP_ASSERT("httpd_init: tcp_listen failed", pcb != NULL);
        altcp_accept(pcb, http_accept);
      }
    }

    This functions is being called while initializing the HTTP Server.
    You can try and assign a specific IP.

    BestRegards,
    OV_Renesas

  • Hello

    I'm still unable to solve the issue with starting the HTTP server in Soft AP mode. Although I have information indicating that the HTTP server is running, it doesn't respond when I try to access the board's Soft AP IP address. Please analyze this issue again and try to help me.

    When the board is in station mode and I start the server in the same way, the server responds to the IP address assigned to the board by the router via DHCP. However, when I put the board in Soft AP mode and set its IP address to, for example, 10.10.0.5, and start the server in the same way, it does not respond!

    Also, I noticed that even in the "Getting Started" example, there is no command for me to explicitly start the HTTP server.

    Best regards,

    df

Reply
  • Hello

    I'm still unable to solve the issue with starting the HTTP server in Soft AP mode. Although I have information indicating that the HTTP server is running, it doesn't respond when I try to access the board's Soft AP IP address. Please analyze this issue again and try to help me.

    When the board is in station mode and I start the server in the same way, the server responds to the IP address assigned to the board by the router via DHCP. However, when I put the board in Soft AP mode and set its IP address to, for example, 10.10.0.5, and start the server in the same way, it does not respond!

    Also, I noticed that even in the "Getting Started" example, there is no command for me to explicitly start the HTTP server.

    Best regards,

    df

Children
  • Hi Df,

    Apologies for the delay.
    Our Wi-Fi Support Engineers tested it on their side and everything works fine.
    We are not sure what is different from your test. It should work and we just build the HTTP Server example on the FreeRTOS SDK v3.9.2.0.
    Please refer on the attached log [COM138]20250626-10_53_11.log

    [2025-06-26 11:23:23.737] [/DA16200/NVRAM] # setup
    [2025-06-26 11:23:24.761] 
    [2025-06-26 11:23:24.761] Stop all services for the setting.
    [2025-06-26 11:23:24.761]  Are you sure ? [Yes/No] : y
    [2025-06-26 11:23:25.165] 
    [2025-06-26 11:23:25.165] 
    [2025-06-26 11:23:25.165] [ DA16200 EASY SETUP ]
    [2025-06-26 11:23:25.174] 
    [2025-06-26 11:23:25.175] Country Code List:
    [2025-06-26 11:23:25.175] AD  AE  AF  AI  AL  AM  AR  AS  AT  AU  AW  AZ  BA  BB  BD  BE  BF  BG  BH  BL  
    [2025-06-26 11:23:25.175] BM  BN  BO  BR  BS  BT  BY  BZ  CA  CF  CH  CI  CL  CN  CO  CR  CU  CX  CY  CZ  
    [2025-06-26 11:23:25.189] DE  DK  DM  DO  DZ  EC  EE  EG  ES  ET  EU  FI  FM  FR  GA  GB  GD  GE  GF  GH  
    [2025-06-26 11:23:25.189] GL  GP  GR  GT  GU  GY  HK  HN  HR  HT  HU  ID  IE  IL  IN  IR  IS  IT  JM  JO  
    [2025-06-26 11:23:25.189] JP  KE  KH  KN  KP  KR  KW  KY  KZ  LB  LC  LI  LK  LS  LT  LU  LV  MA  MC  MD  
    [2025-06-26 11:23:25.189] ME  MF  MH  MK  MN  MO  MP  MQ  MR  MT  MU  MV  MW  MX  MY  NG  NI  NL  NO  NP  
    [2025-06-26 11:23:25.205] NZ  OM  PA  PE  PF  PG  PH  PK  PL  PM  PR  PT  PW  PY  QA  RE  RO  RS  RU  RW  
    [2025-06-26 11:23:25.205] SA  SE  SG  SI  SK  SN  SR  SV  SY  TC  TD  TG  TH  TN  TR  TT  TW  TZ  UA  UG  
    [2025-06-26 11:23:25.205] UK  US  UY  UZ  VA  VC  VE  VI  VN  VU  WF  WS  YE  YT  ZA  ZW  ALL     
    [2025-06-26 11:23:25.205] 
    [2025-06-26 11:23:25.205]  COUNTRY CODE ? [Quit] (Default KR) : 
    [2025-06-26 11:23:25.765] Default Country: KR
    [2025-06-26 11:23:25.797] 
    [2025-06-26 11:23:25.797] SYSMODE(WLAN MODE) ?
    [2025-06-26 11:23:25.797] 	1. Station
    [2025-06-26 11:23:25.797] 	2. Soft-AP
    [2025-06-26 11:23:25.797] 	3. Station & SOFT-AP
    [2025-06-26 11:23:25.797]  MODE ?  [1/2/3/Quit] (Default Station) : 2
    [2025-06-26 11:23:27.192] 
    [2025-06-26 11:23:27.192] [ SOFT-AP CONFIGURATION ]
    [2025-06-26 11:23:27.192] 
    [2025-06-26 11:23:27.192]  SSID ? (Default DA16200_E96AF3) : 
    [2025-06-26 11:23:29.893] 
    [2025-06-26 11:23:29.893]  CHANNEL ? [1~13, Auto:0/Quit] (Default Auto) : 
    [2025-06-26 11:23:31.703] 
    [2025-06-26 11:23:31.703] 
    [2025-06-26 11:23:31.703] AUTHENTICATION ?
    [2025-06-26 11:23:31.703] 	 1. OPEN
    [2025-06-26 11:23:31.703] 	 2. WEP(Unsupported)
    [2025-06-26 11:23:31.703] 	 3. WPA-PSK
    [2025-06-26 11:23:31.703] 	 4. WPA2-PSK (Recommend)
    [2025-06-26 11:23:31.703] 	 5. WPA/WPA2-PSK
    [2025-06-26 11:23:31.703]  AUTHENTICATION ? [1/3/4/5/Quit] : 1
    [2025-06-26 11:23:33.878] 
    [2025-06-26 11:23:33.878] 
    [2025-06-26 11:23:33.878]  Do you want to set advanced WiFi configuration ? [No/Yes/Quit] (Default No) : 
    [2025-06-26 11:23:36.052] ============================================
    [2025-06-26 11:23:36.052] SSID        : DA16200_E96AF3
    [2025-06-26 11:23:36.052] CHANNEL     : AUTO(ACS)
    [2025-06-26 11:23:36.052] AUTH        : OPEN
    [2025-06-26 11:23:36.052] WIFI MODE   : 11b/g/n
    [2025-06-26 11:23:36.052] ============================================
    [2025-06-26 11:23:36.052]  WIFI CONFIGURATION CONFIRM ? [Yes/No/Quit] : 
    [2025-06-26 11:23:36.296]  WIFI CONFIGURATION CONFIRM ? [Yes/No/Quit] : y
    [2025-06-26 11:23:37.590] 
    [2025-06-26 11:23:37.590] 
    [2025-06-26 11:23:37.590]  IP ADDRESS ? [Quit] (Default 10.0.0.1) : 
    [2025-06-26 11:23:38.615] 
    [2025-06-26 11:23:38.615]  SUBNET ? [Quit] (Default 255.255.255.0) : 
    [2025-06-26 11:23:39.543] 
    [2025-06-26 11:23:39.543]  GATEWAY ? [Quit] (Default 10.0.0.1) : 
    [2025-06-26 11:23:40.297] ============================================
    [2025-06-26 11:23:40.297] [WLAN1]
    [2025-06-26 11:23:40.297] IP ADDRESS: 10.0.0.1
    [2025-06-26 11:23:40.297] SUBNET    : 255.255.255.0
    [2025-06-26 11:23:40.297] GATEWAY   : 10.0.0.1
    [2025-06-26 11:23:40.297] ============================================
    [2025-06-26 11:23:40.297]  IP CONFIGURATION CONFIRM ? [Yes/No/Quit] : y
    [2025-06-26 11:23:41.237] 
    [2025-06-26 11:23:41.237] 
    [2025-06-26 11:23:41.237]  DHCP SERVER CONFIGURATION ? [Yes/No/Quit] : y
    [2025-06-26 11:23:42.297] 
    [2025-06-26 11:23:42.297] 
    [2025-06-26 11:23:42.297]  DHCP SERVER LEASE IP Count(MAX 10) ? [Quit] (Default 10) : 
    [2025-06-26 11:23:43.464] 
    [2025-06-26 11:23:43.464]  DHCP SERVER LEASE TIME(60 ~ 86400 SEC) ? [Quit] (Default 1800) : 
    [2025-06-26 11:23:43.654] ============================================
    [2025-06-26 11:23:43.654] [DHCP SERVER]
    [2025-06-26 11:23:43.654] Start IP  : 10.0.0.2
    [2025-06-26 11:23:43.654] END IP    : 10.0.0.11
    [2025-06-26 11:23:43.654] LEASE TIME: 1800
    [2025-06-26 11:23:43.654] ============================================
    [2025-06-26 11:23:43.669] 
    [2025-06-26 11:23:43.669]  DHCP SERVER CONFIGURATION CONFIRM ? [Yes/No/Quit] : 
    [2025-06-26 11:23:43.847] 
    [2025-06-26 11:23:43.847]  DHCP SERVER CONFIGURATION CONFIRM ? [Yes/No/Quit] : y
    [2025-06-26 11:23:44.454] 
    [2025-06-26 11:23:44.535] Configuration OK
    [2025-06-26 11:23:46.822] 
    [2025-06-26 11:23:46.822] Reboot...
    [2025-06-26 11:23:46.822] 
    [2025-06-26 11:23:47.958] 
    [2025-06-26 11:23:47.958] Wakeup source is 0x0 
    [2025-06-26 11:23:47.958] [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    [2025-06-26 11:23:47.974] 
    [2025-06-26 11:23:47.974] 
    [2025-06-26 11:23:47.974] 	******************************************************
    [2025-06-26 11:23:47.974] 	*             DA16200 SDK Information
    [2025-06-26 11:23:47.974] 	* --------------------------------------------------- 
    [2025-06-26 11:23:47.974] 	*
    [2025-06-26 11:23:47.974] 	* - CPU Type        : Cortex-M4 (120MHz)
    [2025-06-26 11:23:47.974] 	* - OS Type         : FreeRTOS 10.4.3
    [2025-06-26 11:23:47.974] 	* - Serial Flash    : 4 MB
    [2025-06-26 11:23:47.974] 	* - SDK Version     : V3.2.9.2 GEN
    [2025-06-26 11:23:47.974] 	* - F/W Version     : FRTOS-GEN01-01-efcbdccd0e-006940
    [2025-06-26 11:23:47.989] 	* - F/W Build Time  : Jun 26 2025 10:49:37
    [2025-06-26 11:23:47.989] 	* - Boot Index      : 0
    [2025-06-26 11:23:47.989] 	*
    [2025-06-26 11:23:47.989] 	******************************************************
    [2025-06-26 11:23:47.989] 
    [2025-06-26 11:23:48.022] 
    [2025-06-26 11:23:48.022] System Mode : Soft-AP (1)
    [2025-06-26 11:23:48.022] 
    [2025-06-26 11:23:48.022] >>> DHCP Server Started
    [2025-06-26 11:23:48.022] >>> Start DA16X Supplicant ...
    [2025-06-26 11:23:48.038] >>> DA16x Supp Ver2.7 - 2022_03
    [2025-06-26 11:23:48.038] >>> Add SoftAP Inteface (softap1) ...
    [2025-06-26 11:23:48.055] >>> MAC address (softap1) : d4:3d:39:e9:6a:f3
    [2025-06-26 11:23:48.055] >>> softap1 interface add OK
    [2025-06-26 11:23:48.055] >>> AP Operating Channel: AUTO
    [2025-06-26 11:23:50.036] >>> Soft-AP ACS : ideal ch is 13
    [2025-06-26 11:23:50.036] 
    [2025-06-26 11:23:50.036] >>> Network Interface (wlan1) : UP
    [2025-06-26 11:23:50.036] >>> BSS Isolate Disabled
    [2025-06-26 11:23:50.036] 
    [2025-06-26 11:23:50.036] Soft-AP is Ready (d4:3d:39:e9:6a:f3)
    [2025-06-26 11:23:50.036] 
    [2025-06-26 11:23:50.036] 
    [2025-06-26 11:23:50.036] >>> Start HTTP-Server sample
    [2025-06-26 11:23:50.036] [http_server_sample] HTTP-Server Start!! 
    [2025-06-26 11:23:50.036] 
    [2025-06-26 11:23:50.036] =======================================================
    [2025-06-26 11:23:50.036] [Start Provisioning with TCP/TLS] .. Soft AP Mode 
    [2025-06-26 11:23:50.051] =======================================================
    [2025-06-26 11:23:50.051] [app_provision_switch_client_thread] Create...(status=0) [1] 
    [2025-06-26 11:23:50.051] [app_provision_TLS_server_thread] Create TLS... 
    [2025-06-26 11:23:50.051] 
    [2025-06-26 11:23:50.051] >>> Start Provisioning Server (TLS) ...
    [2025-06-26 11:23:50.051] [app_provision_TCP_server_thread] Create ... 
    [2025-06-26 11:23:50.195] Wait Accept (TLS)...
    [2025-06-26 11:23:50.835] 
    [2025-06-26 11:23:50.835] > Wi-Fi Scan request success.
    [2025-06-26 11:23:50.835] (0) GoogleNestPoint9CC5.9CC5.ybc, / 3 / -26 / 2432 
    [2025-06-26 11:23:50.852] (1) ASUS_RT_AC1750_7 / 3 / -29 / 2452 
    [2025-06-26 11:23:50.852] (2) RMS-Wifi2 / 3 / -35 / 2462 
    [2025-06-26 11:23:50.852] (3) netis2g / 0 / -35 / 2472 
    [2025-06-26 11:23:50.852] (4) RenesasCSAP / 3 / -36 / 2452 
    [2025-06-26 11:23:50.852] (5) FRITZBox7530VN / 3 / -36 / 2462 
    [2025-06-26 11:23:50.852] (6) 360_F5C_IOP / 3 / -37 / 2437 
    [2025-06-26 11:23:50.852] (7) HUAWEI_WS550 / 3 / -38 / 2437 
    [2025-06-26 11:23:50.852] (8) HiWiFi_5B2310 / 3 / -38 / 2427 
    [2025-06-26 11:23:50.852] (9) REL-GLOBAL / 3 / -39 / 2412 
    [2025-06-26 11:23:50.867] (10) REL-MOBILE / 3 / -40 / 2412 
    [2025-06-26 11:23:50.867] (11) XIAOMI_RA72 / 3 / -40 / 2437 
    [2025-06-26 11:23:50.867] (12) R-GUEST / 0 / -40 / 2412 
    [2025-06-26 11:23:50.867] (13) Tenda_AC23 / 3 / -42 / 2437 
    [2025-06-26 11:23:50.867] (14) FRITZ!Box 5530 MM / 3 / -43 / 2442 
    [2025-06-26 11:23:50.867] (15) ASUS_RT_AX56U_V2 / 0 / -45 / 2437 
    [2025-06-26 11:23:50.867] (16) linksys-tin_2 / 0 / -46 / 2412 
    [2025-06-26 11:23:50.867] (17) Julian_gate / 3 / -47 / 2472 
    [2025-06-26 11:23:50.867] (18) NETIS_WF2003 / 3 / -49 / 2412 
    [2025-06-26 11:23:50.867] (19) NETIS_WF2781 / 3 / -49 / 2452 
    [2025-06-26 11:23:50.884] (20) TPLINK_AX21_KSHAN / 0 / -50 / 2412 
    [2025-06-26 11:23:50.884] (21) MATTER / 0 / -52 / 2447 
    [2025-06-26 11:23:50.884] (22) TPLINK_AX21_Bell / 3 / -53 / 2412 
    [2025-06-26 11:23:50.884] (23) IPTIME_AX2004M_KSHAN / 1 / -55 / 2412 
    [2025-06-26 11:23:50.884] (24) N_TPLINK_EAP620HD_WPA1-ENT-AUTO / 2 / -57 / 2412 
    [2025-06-26 11:23:50.884] (25) N_TPLINK_EAP620HD_WPA3-ENT-128B / 3 / -58 / 2412 
    [2025-06-26 11:23:50.884] (26) N_TPLINK_EAP620HD_WEP-64BIT / 0 / -58 / 2412 
    [2025-06-26 11:23:50.884] (27) N_A1004_OPEN / 0 / -60 / 2437 
    [2025-06-26 11:23:50.884] (28) ASUS_RT_AC1200GU / 0 / -61 / 2447 
    [2025-06-26 11:23:50.900] (29) Belliron_2.4G_OPEN / 0 / -62 / 2437 
    [2025-06-26 11:23:50.900] 
    [2025-06-26 11:23:50.900] [app_provision_TCP_server_thread] socket().. status=1  
    [2025-06-26 11:23:50.900]  Wait Accept...
    [2025-06-26 11:24:01.619] AP-STA-CONNECTED 6c:2f:80:56:7c:78
    [2025-06-26 11:24:29.091] 
    [2025-06-26 11:24:29.091] [/DA16200] # 
    [2025-06-26 11:24:29.268] [/DA16200] # nvram.getenv
    [2025-06-26 11:24:33.217] 
    [2025-06-26 11:24:33.217] Total length (350)
    [2025-06-26 11:24:33.217] tls_ver (STR,04) ............. 769 
    [2025-06-26 11:24:33.217] peap_ver (STR,02) ............ 1 
    [2025-06-26 11:24:33.217] N1_Profile (STR,02) .......... 1 
    [2025-06-26 11:24:33.217] N1_ssid (STR,17) ............. "DA16200_E96AF3" 
    [2025-06-26 11:24:33.217] N1_mode (STR,02) ............. 2 
    [2025-06-26 11:24:33.217] N1_frequency (STR,02) ........ 0 
    [2025-06-26 11:24:33.217] N1_proActKeyCaching (STR,02) . 0 
    [2025-06-26 11:24:33.217] N1_auth_max_failures (STR,02)  3 
    [2025-06-26 11:24:33.217] SYSMODE (STR,02) ............. 1 
    [2025-06-26 11:24:33.233] 1:NETMODE (STR,02) ........... 2 
    [2025-06-26 11:24:33.233] 1:IPADDR (STR,09) ............ 10.0.0.1 
    [2025-06-26 11:24:33.233] 1:NETMASK (STR,14) ........... 255.255.255.0 
    [2025-06-26 11:24:33.233] 1:GATEWAY (STR,09) ........... 10.0.0.1 
    [2025-06-26 11:24:33.233] DHCPD_S_IP (STR,09) .......... 10.0.0.2 
    [2025-06-26 11:24:33.233] DHCPD_E_IP (STR,10) .......... 10.0.0.11 
    [2025-06-26 11:24:33.233] DHCPD_TIME (STR,05) .......... 1800 
    [2025-06-26 11:24:33.233] USEDHCPD (STR,02) ............ 1 
    [2025-06-26 11:24:33.233] [/DA16200/NVRAM] # 
    [2025-06-26 11:24:38.613] [/DA16200/NVRAM] # Received tot_len = 432, len = 432, err = 0 
    [2025-06-26 11:24:41.792] >>>  
    [2025-06-26 11:24:41.792] - (len=432):
    [2025-06-26 11:24:41.792] [00000000]  47 45 54 20 2f 20 48 54 54 50 2f 31 2e 31 0d 0a  GET / HTTP/1.1..
    [2025-06-26 11:24:41.792] [00000010]  48 6f 73 74 3a 20 31 30 2e 30 2e 30 2e 31 0d 0a  Host: 10.0.0.1..
    [2025-06-26 11:24:41.792] [00000020]  43 6f 6e 6e 65 63 74 69 6f 6e 3a 20 6b 65 65 70  Connection: keep
    [2025-06-26 11:24:41.792] [00000030]  2d 61 6c 69 76 65 0d 0a 55 70 67 72 61 64 65 2d  -alive..Upgrade-
    [2025-06-26 11:24:41.792] [00000040]  49 6e 73 65 63 75 72 65 2d 52 65 71 75 65 73 74  Insecure-Request
    [2025-06-26 11:24:41.809] [00000050]  73 3a 20 31 0d 0a 55 73 65 72 2d 41 67 65 6e 74  s: 1..User-Agent
    [2025-06-26 11:24:41.809] [00000060]  3a 20 4d 6f 7a 69 6c 6c 61 2f 35 2e 30 20 28 57  : Mozilla/5.0 (W
    [2025-06-26 11:24:41.809] [00000070]  69 6e 64 6f 77 73 20 4e 54 20 31 30 2e 30 3b 20  indows NT 10.0; 
    [2025-06-26 11:24:41.809] [00000080]  57 69 6e 36 34 3b 20 78 36 34 29 20 41 70 70 6c  Win64; x64) Appl
    [2025-06-26 11:24:41.825] [00000090]  65 57 65 62 4b 69 74 2f 35 33 37 2e 33 36 20 28  eWebKit/537.36 (
    [2025-06-26 11:24:41.825] [000000a0]  4b 48 54 4d 4c 2c 20 6c 69 6b 65 20 47 65 63 6b  KHTML, like Geck
    [2025-06-26 11:24:41.825] [000000b0]  6f 29 20 43 68 72 6f 6d 65 2f 31 33 32 2e 30 2e  o) Chrome/132.0.
    [2025-06-26 11:24:41.825] [000000c0]  30 2e 30 20 53 61 66 61 72 69 2f 35 33 37 2e 33  0.0 Safari/537.3
    [2025-06-26 11:24:41.825] [000000d0]  36 0d 0a 41 63 63 65 70 74 3a 20 74 65 78 74 2f  6..Accept: text/
    [2025-06-26 11:24:41.841] [000000e0]  68 74 6d 6c 2c 61 70 70 6c 69 63 61 74 69 6f 6e  html,application
    [2025-06-26 11:24:41.841] [000000f0]  2f 78 68 74 6d 6c 2b 78 6d 6c 2c 61 70 70 6c 69  /xhtml+xml,appli
    [2025-06-26 11:24:41.841] [00000100]  63 61 74 69 6f 6e 2f 78 6d 6c 3b 71 3d 30 2e 39  cation/xml;q=0.9
    [2025-06-26 11:24:41.857] [00000110]  2c 69 6d 61 67 65 2f 61 76 69 66 2c 69 6d 61 67  ,image/avif,imag
    [2025-06-26 11:24:41.857] [00000120]  65 2f 77 65 62 70 2c 69 6d 61 67 65 2f 61 70 6e  e/webp,image/apn
    [2025-06-26 11:24:41.857] [00000130]  67 2c 2a 2f 2a 3b 71 3d 30 2e 38 2c 61 70 70 6c  g,*/*;q=0.8,appl
    [2025-06-26 11:24:41.857] [00000140]  69 63 61 74 69 6f 6e 2f 73 69 67 6e 65 64 2d 65  ication/signed-e
    [2025-06-26 11:24:41.857] [00000150]  78 63 68 61 6e 67 65 3b 76 3d 62 33 3b 71 3d 30  xchange;v=b3;q=0
    [2025-06-26 11:24:41.872] [00000160]  2e 37 0d 0a 41 63 63 65 70 74 2d 45 6e 63 6f 64  .7..Accept-Encod
    [2025-06-26 11:24:41.872] [00000170]  69 6e 67 3a 20 67 7a 69 70 2c 20 64 65 66 6c 61  ing: gzip, defla
    [2025-06-26 11:24:41.872] [00000180]  74 65 0d 0a 41 63 63 65 70 74 2d 4c 61 6e 67 75  te..Accept-Langu
    [2025-06-26 11:24:41.873] [00000190]  61 67 65 3a 20 65 6e 2d 55 53 2c 65 6e 3b 71 3d  age: en-US,en;q=
    [2025-06-26 11:24:41.889] [000001a0]  30 2e 39 2c 6b 6f 3b 71 3d 30 2e 38 0d 0a 0d 0a  0.9,ko;q=0.8....
    [2025-06-26 11:24:41.889] Received tot_len = 370, len = 370, err = 0 
    [2025-06-26 11:24:41.889] >>>  
    [2025-06-26 11:24:41.889] - (len=370):
    [2025-06-26 11:24:41.889] [00000000]  47 45 54 20 2f 69 6d 67 2f 73 69 63 73 2e 67 69  GET /img/sics.gi
    [2025-06-26 11:24:41.889] [00000010]  66 20 48 54 54 50 2f 31 2e 31 0d 0a 48 6f 73 74  f HTTP/1.1..Host
    [2025-06-26 11:24:41.889] [00000020]  3a 20 31 30 2e 30 2e 30 2e 31 0d 0a 43 6f 6e 6e  : 10.0.0.1..Conn
    [2025-06-26 11:24:41.905] [00000030]  65 63 74 69 6f 6e 3a 20 6b 65 65 70 2d 61 6c 69  ection: keep-ali
    [2025-06-26 11:24:41.905] [00000040]  76 65 0d 0a 55 73 65 72 2d 41 67 65 6e 74 3a 20  ve..User-Agent: 
    [2025-06-26 11:24:41.905] [00000050]  4d 6f 7a 69 6c 6c 61 2f 35 2e 30 20 28 57 69 6e  Mozilla/5.0 (Win
    [2025-06-26 11:24:41.905] [00000060]  64 6f 77 73 20 4e 54 20 31 30 2e 30 3b 20 57 69  dows NT 10.0; Wi
    [2025-06-26 11:24:41.905] [00000070]  6e 36 34 3b 20 78 36 34 29 20 41 70 70 6c 65 57  n64; x64) AppleW
    [2025-06-26 11:24:41.920] [00000080]  65 62 4b 69 74 2f 35 33 37 2e 33 36 20 28 4b 48  ebKit/537.36 (KH
    [2025-06-26 11:24:41.920] [00000090]  54 4d 4c 2c 20 6c 69 6b 65 20 47 65 63 6b 6f 29  TML, like Gecko)
    [2025-06-26 11:24:41.920] [000000a0]  20 43 68 72 6f 6d 65 2f 31 33 32 2e 30 2e 30 2e   Chrome/132.0.0.
    [2025-06-26 11:24:41.920] [000000b0]  30 20 53 61 66 61 72 69 2f 35 33 37 2e 33 36 0d  0 Safari/537.36.
    [2025-06-26 11:24:41.937] [000000c0]  0a 41 63 63 65 70 74 3a 20 69 6d 61 67 65 2f 61  .Accept: image/a
    [2025-06-26 11:24:41.937] [000000d0]  76 69 66 2c 69 6d 61 67 65 2f 77 65 62 70 2c 69  vif,image/webp,i
    [2025-06-26 11:24:41.937] [000000e0]  6d 61 67 65 2f 61 70 6e 67 2c 69 6d 61 67 65 2f  mage/apng,image/
    [2025-06-26 11:24:41.954] [000000f0]  73 76 67 2b 78 6d 6c 2c 69 6d 61 67 65 2f 2a 2c  svg+xml,image/*,
    [2025-06-26 11:24:41.954] [00000100]  2a 2f 2a 3b 71 3d 30 2e 38 0d 0a 52 65 66 65 72  */*;q=0.8..Refer
    [2025-06-26 11:24:41.954] [00000110]  65 72 3a 20 68 74 74 70 3a 2f 2f 31 30 2e 30 2e  er: http://10.0.
    [2025-06-26 11:24:41.954] [00000120]  30 2e 31 2f 0d 0a 41 63 63 65 70 74 2d 45 6e 63  0.1/..Accept-Enc
    [2025-06-26 11:24:41.954] [00000130]  6f 64 69 6e 67 3a 20 67 7a 69 70 2c 20 64 65 66  oding: gzip, def
    [2025-06-26 11:24:41.969] [00000140]  6c 61 74 65 0d 0a 41 63 63 65 70 74 2d 4c 61 6e  late..Accept-Lan
    [2025-06-26 11:24:41.969] [00000150]  67 75 61 67 65 3a 20 65 6e 2d 55 53 2c 65 6e 3b  guage: en-US,en;
    [2025-06-26 11:24:41.969] [00000160]  71 3d 30 2e 39 2c 6b 6f 3b 71 3d 30 2e 38 0d 0a  q=0.9,ko;q=0.8..
    [2025-06-26 11:24:41.969] [00000170]  0d 0a                                            ..              
    [2025-06-26 11:24:41.985] Received tot_len = 369, len = 369, err = 0 
    [2025-06-26 11:24:41.985] >>>  
    [2025-06-26 11:24:41.985] - (len=369):
    [2025-06-26 11:24:41.985] [00000000]  47 45 54 20 2f 66 61 76 69 63 6f 6e 2e 69 63 6f  GET /favicon.ico
    [2025-06-26 11:24:41.985] [00000010]  20 48 54 54 50 2f 31 2e 31 0d 0a 48 6f 73 74 3a   HTTP/1.1..Host:
    [2025-06-26 11:24:41.985] [00000020]  20 31 30 2e 30 2e 30 2e 31 0d 0a 43 6f 6e 6e 65   10.0.0.1..Conne
    [2025-06-26 11:24:41.985] [00000030]  63 74 69 6f 6e 3a 20 6b 65 65 70 2d 61 6c 69 76  ction: keep-aliv
    [2025-06-26 11:24:42.004] [00000040]  65 0d 0a 55 73 65 72 2d 41 67 65 6e 74 3a 20 4d  e..User-Agent: M
    [2025-06-26 11:24:42.004] [00000050]  6f 7a 69 6c 6c 61 2f 35 2e 30 20 28 57 69 6e 64  ozilla/5.0 (Wind
    [2025-06-26 11:24:42.004] [00000060]  6f 77 73 20 4e 54 20 31 30 2e 30 3b 20 57 69 6e  ows NT 10.0; Win
    [2025-06-26 11:24:42.004] [00000070]  36 34 3b 20 78 36 34 29 20 41 70 70 6c 65 57 65  64; x64) AppleWe
    [2025-06-26 11:24:42.022] [00000080]  62 4b 69 74 2f 35 33 37 2e 33 36 20 28 4b 48 54  bKit/537.36 (KHT
    [2025-06-26 11:24:42.022] [00000090]  4d 4c 2c 20 6c 69 6b 65 20 47 65 63 6b 6f 29 20  ML, like Gecko) 
    [2025-06-26 11:24:42.022] [000000a0]  43 68 72 6f 6d 65 2f 31 33 32 2e 30 2e 30 2e 30  Chrome/132.0.0.0
    [2025-06-26 11:24:42.022] [000000b0]  20 53 61 66 61 72 69 2f 35 33 37 2e 33 36 0d 0a   Safari/537.36..
    [2025-06-26 11:24:42.022] [000000c0]  41 63 63 65 70 74 3a 20 69 6d 61 67 65 2f 61 76  Accept: image/av
    [2025-06-26 11:24:42.039] [000000d0]  69 66 2c 69 6d 61 67 65 2f 77 65 62 70 2c 69 6d  if,image/webp,im
    [2025-06-26 11:24:42.039] [000000e0]  61 67 65 2f 61 70 6e 67 2c 69 6d 61 67 65 2f 73  age/apng,image/s
    [2025-06-26 11:24:42.039] [000000f0]  76 67 2b 78 6d 6c 2c 69 6d 61 67 65 2f 2a 2c 2a  vg+xml,image/*,*
    [2025-06-26 11:24:42.039] [00000100]  2f 2a 3b 71 3d 30 2e 38 0d 0a 52 65 66 65 72 65  /*;q=0.8..Refere
    [2025-06-26 11:24:42.050] [00000110]  72 3a 20 68 74 74 70 3a 2f 2f 31 30 2e 30 2e 30  r: http://10.0.0
    [2025-06-26 11:24:42.050] [00000120]  2e 31 2f 0d 0a 41 63 63 65 70 74 2d 45 6e 63 6f  .1/..Accept-Enco
    [2025-06-26 11:24:42.050] [00000130]  64 69 6e 67 3a 20 67 7a 69 70 2c 20 64 65 66 6c  ding: gzip, defl
    [2025-06-26 11:24:42.050] [00000140]  61 74 65 0d 0a 41 63 63 65 70 74 2d 4c 61 6e 67  ate..Accept-Lang
    [2025-06-26 11:24:42.050] [00000150]  75 61 67 65 3a 20 65 6e 2d 55 53 2c 65 6e 3b 71  uage: en-US,en;q
    [2025-06-26 11:24:42.069] [00000160]  3d 30 2e 39 2c 6b 6f 3b 71 3d 30 2e 38 0d 0a 0d  =0.9,ko;q=0.8...
    [2025-06-26 11:24:42.069] [00000170]  0a                                               .               
    

    We then checked again for the specific IP of 10.10.0.1 and it works as well:


    If you could provide your image (FRTOS) or the whole SDK, we could try to recreate your issue.

    We would also like to suggest checking for the ping test if it is reachable or not. It could be good to test with mobile or another PC.
    Please refer on UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide section 6.2 Ping test.


    Best Regards,
    OV_Renesas

  • Hi,

    It's working now! The issue was that I hadn't configured DHCP for Soft AP mode, which likely caused a conflict with IP addresses. Now everything is working fine.

    Thank you again - I really appreciate your great support.

    Best regards,

    df