使用e2studio,e1仿真器调试rh850 F1KM-S4-V3时报错。
调试的配置信息如下所示:
具体的报错信息如下所示:
GDB Server for Renesas targets.
Version 10.0.0.v20241002-021700 [fe04c343] (Oct 2 2024 18:08:08)
Starting server with the following options:
Raw options : C:\Users\16563\.eclipse\com.renesas.platform_1435879475\DebugComp\\RH850\e2-server-gdb -g E1 -t R7F701649 -uConnectionTimeout= 30 -umFreq= 8.00 -ulpdType= 4 -ulpdFreq= Default -setOptJtagLpd= 1 -setOptJtagJtag= 0 -w 0 -usecurityID= FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF -uneedAuthentication= 0 -uresetOnReload= 1 -ustopPeriEmu= 0 -umaskReset= 0 -umaskHldrq= 0 -umaskStop= 0 -umaskWait= 0 -uverifyOnWritingMemory= 0 -uWorkRamAddress= 0xfedfda00 -uForceReset= 0 -uUseSyncTrace= 0 -l -uCore= SINGLE_CORE|enabled|1|main -uSyncMode= async -uFirstGDB= main --gdbVersion= 7.2
Connecting to RH850 Target
GDBServer endian : little
Starting target connection
Version Information:
GDB action 'connect to target', has failed with error code, 0x00000ccb
force_kill_gdb()
Disconnected from the Target Debugger.
请问该如何解决这个问题,谢谢。