RL78 下载调试

调试无法点击运行,会一直卡在主函数第一行,错误信息如下:GDB action 'go', has failed with error report, Can not write the flash memory because the clock frequency is beyond the limits of regulations.\nIt may be avoidable by the following setting change or processing change. \n- Select the frequency value of the External clock source with a "Main Clock Frequency[MHz]".\n- Select the "System" with a "Monitor clock".\n- Change from a system clock to a main clock by SFR rewriting.

Parents Reply Children
No Data