How To Debug the ICUM of P1X-C in CS+?
Chip:137X
I have developed the ELFprograms for ICUM and PE.: Host.elf and Icum.elf. I have an E2 debugger
i have a DR7F701374I.dvf
Hi Snikeguo,
P1X-C is part of the RH850 serial, and you can select the E2 as debugger in CS+:
hello support:When i enable ICUM(by modify secuity setting area) ,how to disable ICUM ?When I modify secuity setting area(0xff322700-0xff32730) to fill 0xFF,it can not be modified,like this(from read memory)
using GHS to write flash :error num 0xc28