RA6M4_FreeRTOS_FAT USB读写U盘长短文件名异常问题

Hi:

长文件名称文件USB输出到U盘有错,13个字符文件名输出是正常的。长度超出13个字符后文件名显示乱码。

 

1.FreeRTOS+FAT配置如下

2.文件名长度超出13个字符后,文件名显示乱码。

3.单步仿真查看写入之前用的文件名内容是对的,通过文件系统写入到U盘后,文件名就显示为乱码.

Tips: e2studio里用FSP V5.1和V5.5测试是相同问题。

Parents Reply Children