rzg2l M33编译烧入问题

NPE doesn’t be able to flash the M33 using JTAG.
The SOM on the DemoBoard is programmed with the image obtained from the SDK rzg2l-yocto-sdk3.0.5 integrating the multi-os part that
I get this type of error.