NPE doesn’t be able to flash the M33 using JTAG.The SOM on the DemoBoard is programmed with the image obtained from the SDK rzg2l-yocto-sdk3.0.5 integrating the multi-os part that I get this type of error.
要进入调试模式,必须在 uboot 中启动,停止 uboot 中的启动过程,然后启动调试会话。
你好,没有明白。
有M33的 JTAG调试和相关资料吗
请参考此文章4.3.2章Release Note for RZ/G Multi-OS Package V1.21 (renesas.com)