在 rpmsg_demo.c 源代码中,如何装载 CM33 端的有用数据发回 CA55 处理器?demo 是把收到的数据发回主处理器。
static int rpmsg_endpoint_cb0 (struct rpmsg_endpoint * cb_rp_ept, void * data, size_t len, uint32_t src, void * priv)
{
/* service 0 */
(void) priv;
(void) src;
/* On reception of a shutdown we signal the application to terminate */
if ((*(unsigned int *) data) == SHUTDOWN_MSG)
evt_svc_unbind[0] = 1;
return RPMSG_SUCCESS;
}
/* Send data back to master */
if (rpmsg_send(cb_rp_ept, data, (int) len) < 0)
LPERROR("rpmsg_send failed\n");
return -1;
static int rpmsg_endpoint_cb1 (struct rpmsg_endpoint * cb_rp_ept, void * data, size_t len, uint32_t src, void * priv)
/* service 1 */
evt_svc_unbind[1] = 1;
此问题我们在另外一个帖子中继续讨论:(1) A55 与 CM33核间通讯 - RZ/G2 Forum - RZ MPU (CN) - Renesas Engineering Community