hi dialog: 目前我这边遇到如下一个问题有关DA14585的,在SDK6.02的pxp_reporter工程默认代码上面不管是仿真还是下载程序到RAM程序都是可以正常运行的,但是在SDK6.04上面运行pxp_reporter这个默认工程,程序代码BUG掉了。目前我这边仿真调试BUG在如下位置arch_rom.c文件的arch_rom_init函数的 // Mandatory HCI root table setup memcpy(hci_cmd_desc_root_tab, rom_hci_cmd_desc_root_tab, 48);(文件的53行) 异常错误为: if ((GetWord16(SYS_STAT_REG) & DBG_IS_UP) == DBG_IS_UP) __asm("BKPT #0\n"); 目前官方提供的代码编译都存在如上问题,还请帮忙分析是什么地方需要改进的。不然别的客户在使用pxp_reporter一定会存在同样问题的.