参照文档通过iperf工具进行吞吐量测试,注意到在配置为AP模式时,测试速率有所提升,但最高仍不超过20Mbps,配置AP模式时使用的是默认配置,即802.11n标准,理论上此标准能达到更高的传输速率。文档中提到TX与RX射频测试,需要在屏蔽环境使用射频连接器和RF线缆进行测试,或许能达到更高的速率,但考虑在日常环境下的信号干扰,并且进行TCP传输时,能否达到更高的传输速率?
关于提高吞吐 有如下建议:
If there is a requirement to increase throughput we will provide these two optimizations:
你好,我使用的是DA16200_DA16600_SDK_FreeRTOS_v3.2.8.1,请问#define TCP_WND这部分定义出现在哪个文件?
你好,麻烦检查一下我私信给你的问题。我这边检索一下TCP_WND的定义位置,稍后回复您