E2 Lite Programmer doesn't seem to work in e2 studio. Clicking debug gives "Error 0x00040102: Not connected to the user system"

I'm using the E2 lite to try to program the RE01 pn: R7F0E01182DNG#AA0. I checked the signals with a logic analyzer (SWDIO SWDCLK, RES) and none of them are toggling at all before the error occurs, so I don't think it's a wiring issue.

The chip has power (not through the programmer), and the VCC light on the e2 lite is on.

The reset led goes on and off when I manually reset the chip so I'm certain that at least the reset pin is connected to the right pin on the e2 lite. I'm confident about the others as well, I've checked and rechecked them.

I also ran the self test program for the e2 lite and it passed.

This is my minimal circuit:



Any help would be greatly appreciated. I've been trying to get this damn chip to take a program for weeks.