This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

RE01 R7F0E015D2CFP#AA1 Setting the Option-Setting Memory

The following is the description of the manual:

Setting Data for Programming Option-Setting Memory :

(1) Changing the Option-Setting Memory by Self-Programming

(2) Debugging through an OCD or Programming by a Flash Memory Writer

The manual describes OFS registers as read-only, so how to set them?

The manual says that there are two methods for setting the above, is there a more detailed sample and step description,

Thank you!