DA9062 Voltages from Buck Regs are higher than desired

I'm using all 4 buck regulators and one of the LDO. The LDO output voltage is perfect but all 4 of the buck regulators output voltages are higher than configured. For example 1.0V is actually 1.2V, 3.3V is actually 3.8V

I noticed that the reference cap value on page 28 table 20 of datasheet is 2.2 uF while on page 61 table 34 recommends 220 nF (or 0.22 uF). Which is the correct value? Is this component critical? Can it be causing the voltage errors I'm seeing?

Parents Reply Children
No Data