ZMOD4410 I2C circuit diagram

Hello, I can not find out ZMOD4410 I2C circuit diagram. How can I design the ZMOD4410  I2C circuit diagram??? 

 If the below figure is the circuit diagram, what is the meaning of Algorithms post-processing?

Algorithms post-processing is it the MCU?

So do I need to connect any resistor or capacitor with VDD or SDA & SCL pin?

Thank you.