SGAS701 footprint

In the datasheet for the sensor there is an outline drawing but no footprint information.

Are there simply 4 pin in a square pattern at 5,08mm pitch (like the classic TO-39) or is it different?

Also, figure 2 with the pin assigment is seen from above, right?