Integrating RH850 Codbase in CI/CD Pipeline

Hi,

We currently use the RH850 line of controllers for our project.

I want to integrate my build as part of a CI/CD Pipeline.

I was wondering how I could go about executing the build using the Linux command line so that I can integrate the build in the pipeline.

I'm currently exploring Gitlab CI since my source code is already hosted there.

Thanks.