SPI memory erasing error

由于芯片紧缺,将原先使用da14586改成了da14585,因此需要额外添加一个flash芯片,然后根据586流出的引脚的资源,将spi的4个引脚定义为了:P0_4,P3_0,P0_5,P2_1,CLK,EN,DI,DO,然后打板回来后发现板子能够连接上toolbox,但是执行erase或者其它操作内存的指令时会出现:SPI memory erasing error 的错误,我试着改了toolbox中的引脚定义和flash_programmer.bin,但是都没有起作用,所以我想问的是,怎样才能解决这个问题呢?

感谢