DA16200: Is there a way to set the Keep-Alive of the MQTT Server (AWS MQTT Broker) using DA Module ?

Hi Renesas Team,

I am  using the Dialog Module DA16200 connected to a Host MCU for MQTT.

DA16200 is used as an MQTT Client in this project.

I had configured the dialog module to wake up from DPM and  ping the MQTT Server(AWS Broker) every 10 minutes to the server to keep the connection alive.

For this I programmed the Host MCU to send the AT command "AT+NWMQPING=600" to configure this.

The pings are working fine. However, the AWS MQTT Broker disconnects the connection with DA Module after 5 minutes.

This means that there is a disconnection between AWS MQTT Broker and DA Module from the 6th Minute to the 10th Minute. 

It seems that the Keep-Alive of the AWS MQTT Broker is set at 5 minutes instead of 10. 

My question is: Is there a way to set the Keep Alive of AWS MQTT Broker using DA Module to the desired value of 10 minutes?

Thank you so much for your support,

Regards,

Nandagopal

Parents Reply Children